The internal electronics of the PTI-S pressure transmitter (model accuracy 0.25%) will be updated to use the same chassis as the 0.50% accuracy model.
All PTI-S models, regardless of accuracy class, will have the same frame dimensions. There will be no change to the operation of the product, the change visible to the customer will only affect the A dimension of the product. See table above.
Reasons for the change:
For more information , please contact our sales team:
+358 9 777 1110